PKR39809-02

Compact

 
 

Stainless steel/Mild steel

2–Point locking

1 customer trays

Dimensions

Cubicle height 730 mm

Cubicle width 435 mm

Cubicle depth 352 mm

Figure 3
Compact cubicle with setVUE O.I.

Figure 3 shows an PowerLogic ADVC Controller with a setVUEO.I. housed in a compact control cubicle. The door is held open with the door stay mechanism. The standard equipment tray has been temporarily relocated to the commissioning bracket for accessibility. This is also a feature of the ultra cubicle. Note the terminal block on the DIN rail at the bottom of the tray and the two point locking mechanism on the door.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.