PKR39809-02

Sync Check Feature Selection

If the Sync Check function is required to be used it must firstly be made available.

This can be done in WSOS on the Feature Selection page:

Display > Configuration > Feature Selection > Protection. (ACR)

Display > Configuration > Feature Selection > Detection. (AS)

Sync Check can also be made available for an ACR or AS on the O.I.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.