PKR39809-02

Conditional Auto Reclose

Conditional Auto Reclose is a means of inhibiting an automatic reclose operation unless a predetermined condition has been met.

This feature works in conjunction with an IOEX card and requires a custom IOEX mapping file incorporating two dedicated database points.

  • One database point indicates the ACR’s intent to trip.

  • The second database point will block reclose operations if not asserted.

There is a maximum time that can elapse between when the ACR trips and when a conditional auto reclose can occur, otherwise the ACR will go to lockout.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.