PKR39809-02

Quick Keys

The Quick Keys consist of four user configurable keys that provide the capability for the operator to quickly access commonly used settings without having to navigate to the relevant page on the display.

The default configuration for these keys is shown below.

Figure 21
Default setVUE O.I. Quick Keys

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.