PKR39809-02

Re-Entering the Protection Menu

If the operator exits the Protection Menu without activating the saved settings, when the Protection Menu is re-entered at a later point in time, providing the settings haven’t been put into service by an O.I. shutdown, the process will run through the same activation sequence as shown in Exiting the Protection Menu.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.