PKR39809-02

Introduction to WSOS

Basic configuration of the PowerLogic ADVC Controller can be performed by either the O.I. or using the WSOS software. Some advanced features can only be configured through WSOS.

WSOS is an alternative PowerLogic ADVC Controller interface. It is a software package, based on Microsoft Windows®, for a Personal Computer (PC) that allows management, control, and monitoring of a population of PowerLogic ADVC controller.

WSOS provides easy access to all switchgear functions from opening/closing, configuring protection and communication parameters through to accessing measurement and analytical data. By using a desktop or portable PC, engineers can manage many devices either remotely through a communications link or locally through a serial, USB or Ethernet connection.

WSOS provides:

  • Local language support

  • Advanced controller support

  • SCADA communications capture tool

  • Controller firmware loading

  • Switchgear explorer

  • Launch pad

  • Switchgear status

  • Event log and filtering

  • Feature selection page

  • Setting pages

WSOS provides facilities for

  • Online and offline management of all protection settings.

  • Tripping and Closing of the switchgear and other operator control functions.

  • Uploading of historical data (for example, event record or demand measurements) to the computer, which can be taken away and processed elsewhere.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.