PKR39809-02

System Measurements (AS)

The values shown on the System Measurements page for current and voltage are averaged over the three phases.

System Measurements

 

Average Phase Current

D

Total Power P

1900 kW

D

Average Phase Voltage

D

Total Power Q

200 kVAR

D

Frequency 50.0 Hz

D

PF

0.98

D

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.