PKR39809-02

Exiting the Protection Menu

The operator will not be prompted to ACTIVATE the settings again until they try to exit the Protection menu, when the following screen will appear:

Pressing the Right arrow key will display the following screen:

When the operator scrolls to YES and presses SELECT, the settings are put in service. If the operator scrolls to NO and presses the SELECT key, the following message is displayed: (scrolling)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.