PKR39809-02

Step 1 – Check that DNP3 is Available

The DNP3 communications protocol is available in the PowerLogic ADVC Controller Range by default. Otherwise it can be made available through Feature Selection in WSOS at:

Display > Configuration > Feature Selection > Communications.

NOTE: If DNP3 is required to run on an Ethernet port, TCP/IP must also be made available.

DNP3 can also be made available via the operator interface.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.