PKR39809-02

SF6 Gas Pressure Measurements

Gas pressure measurement is only available when the switchgear for an ACR or AS uses SF6 as the insulating medium, that is RL Series switchgear.

Parameter Value
RL Series

Nominal pressure at 20 °C

105 kPa gauge at 25 °C

Gas pressure display resolution

1 kPa

Gas pressure display accuracy

± 10 kPa

Gas high alarm setting

65 kPa gauge at 25 °C

Gas low alarm setting

± 10 kPa

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.