PKR39809-02

Auto Reclose

When Directional Protection is On, each protection group has its own Auto Reclose On/Off setting.

An automatic reclose will only occur following a protection trip if:

  • Auto Reclose is On for the protection group that was active for that trip, and

  • The global Auto Reclose setting was On.

The global Auto Reclose setting is the usual setting found in WSOS on the Control page or on the operator interface.

Once the Global Auto Reclose setting is On, the forward and reverse Auto Reclose settings can be configured independently. So it’s possible to configure just forward or reverse protection for auto reclose as well as both.

In WSOS, the Forward and Reverse Auto Reclose settings can be found on the Global Settings page for Forward and Reverse protection groups respectively.

As well as on the operator interface.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.