PKR39809-02

Configurable Unsolicited NULL Message

As per the DNP3 standard, any Server that supports Unsolicited response will send out an initial Unsolicited NULL Response to Client, publishing this capability.

With version A50-07.01, sending of this initial response is now made configurable. This configuration is available on the Unsolicited page in WSOS5 5.16.15.

Figure 70
Unsolicited NULL Response

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.