PKR39809-02

Uplifted Phase Pickup Threshold

If the measured phase–ground/earth voltage on any two phases exceeds the Uplifted Phase Pickup Threshold setting value it will trigger a GFN pickup condition.

This setting monitors the phase–ground/earth voltage for any of the two un-faulted phases. Generally, this voltage setting must be more than the nominal phase–ground/earth voltage.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.