PKR39809-02

Launching the Protocol Configuration Tool

The Protocol Configuration Tool can be launched by selecting configurable protocols in the WSOS customize menu when WSOS is off-line.

This will open the protocol configuration dialogue box shown below:

Figure 39
WSOS Protocol Configuration page

Choose New or Existing depending on whether a new protocol mapping file is being created or an existing file is being opened.

Choose Platform> PowerLogic ADVC for PowerLogic ADVC3 controllers.

The protocol configuration tool supports:

  • DNP3

  • IEC 60870-5-101/4

  • Modbus

For PowerLogic ADVC controllers complete the setup information and select OK.

NOTE: When reusing an existing protocol map, please check that the firmware version in the controller is equal to or higher than the firmware version that the map was created for.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.