PKR39809-02

High Vzps Alarm

The Directional Blocking facility includes a High ZPS Voltage alarm. This indication can be useful in unearthed neutral networks for earth fault detection.

The high Vzps alarm is asserted whenever the Alarm Set-point is exceeded for the Alarm Timeout period. Regardless of whether SEF protection is picked up or not. The alarm is cleared when Vzps falls below the Alarm Set-point again.

The High Vzps Alarm can be turned on and configured via WSOS on the Directional Blocking page.

Figure 164
WSOS High VZPS Alarm settings

High Vzps Alarm can also be configured on the operator interface.

The alarm status is displayed by WSOS on the Control page under Controller Status as well as on the operator interface.

The High VZPS alarm is available for transmission by telemetry protocols.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.