PKR39809-02

Power

Real power, reactive power and PF per phase.

  • A Phase

    • Real power; Reactive power; PF

  • B Phase

    • Real power; Reactive power; PF

  • B Phase

    • Real power; Reactive power; PF

NOTE: Energy (Power Meter) readings are not displayed on the setVUE O.I. They are only displayed on the flexVUE O.I. and in WSOS.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.