PKR39809-02

Making Hit and Run Available

Hit and Run can only be made available via WSOS and then needs to be activated at the O.I. before it can be used. So even though it may have been made available, the local operator can choose whether or not to use it. There is no change to the local operator trip/close operation of the device when Hit and Run is turned OFF. When Hit and Run has been made available, the page below will appear towards the end of the system status menu.

Both settings have a range of: OFF, 10...120 s (increments of 5 s). The factory defaults are OFF. Trip and Close delays can have different time settings or one or both can be OFF.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.