PKR39809-02

Active Trip

While the Global Protection Settings determine if a protection pickup has occurred, the time to trip is determined by which trip is active at the time.

At any given time, a trip is active for each element. The active trip depends on whether Auto Reclose is on and if it is on, where any sequence in progress is up to.

If Auto Reclose is off, then the Single Shot trip is active. Even if Auto Reclose is on, the Single Shot trip will be active for the Single Shot Reset Time following a manual close. The Work Tag trip is always active if the Work Tag is applied.

The table below shows which trip is active when the associated settings are applied and at which point in an automatic reclose sequence. Assumes 4 Trips to Lockout.

Table 24 Active Trip Conditions

Active Trip

Auto Reclose

Work Tag

Active when..

Trip 1

ON

OFF

No sequence is in progress.

Trip 2

ON

OFF

Sequence has advanced one trip.

Trip 3

ON

OFF

Sequence has advanced two trips.

Trip 4

ON

OFF

Sequence has advanced three trips.

Single Shot

OFF

OFF

Always

ON

OFF

For SS Reset Time following a manual close.

Work Tag

ON or OFF

ON

Always

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.