PKR39809-02

Normal Local/Remote Operation

When the PowerLogic ADVC Controller is in Local control mode, certain SCADA binary controls are disabled (off-line). They are:

  • Switchgear Close

  • Work Tag On

  • Work Tag Off

All binary controls as well as all analogue controls are on-line when the PowerLogic ADVC Controller is in Remote control mode.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.