PKR39809-02

Default Configuration

The Status Lamps are programmed in the factory to a default configuration.

The default configuration is shown below. Each lamp indicates the state of the function described next to it. When a state is active, the lamp is lit.

For example, when the recloser is in Lockout the lamp next to Lockout in position a-1 will be on.

Conversely if the lamp is off, the recloser is not in a lockout state.

It is possible that more than one lamp will be lit at a given time.

Example, when a recloser tripped to lockout due to an over current fault on Phase A, both Lockout (a-1) and A-Phase O/C (a-2) lamps will be lit.

Figure 16
flexVUE O.I. Status lamps

The table below describes the default function and color of each lamp.

Table 3 flexVUE Status Lamp descriptions

LED No. Color Description Possible causes
Column A
a-1

Red

Lockout

Recloser has tripped to lockout due to a protection sequence or operator command. Automatic close operations are not possible and the operator has to close the recloser using the O.I. or a remote command.

a-2

Red

A-Phase O/C

The most recent trip of the recloser was caused by an over current event due to a fault on the relevant network phases.

a-3

Red

B-Phase O/C

a-4

Red

C-Phase O/C

a-5

Red

Ground Fault

The most recent trip was caused by a ground (earth) fault.

a-6

Red

Sensitive Ground

The most recent trip was caused by a sensitive ground (earth) fault.

Column B

b-1

Red

Pickup

One of the protection elements detected a value outside the normal range, for example when the phase current exceeds the phase trip setting value.

b-2

Red

Reverse Fault

Protection has operated in the reverse direction due to power flow from the load side to the source side of the recloser.

b-3

Red

O/U Frequency

An over or under frequency event has caused the recloser to trip.

b-4

Red

O/U Voltage

An over or under voltage event has caused the recloser to trip.

b-5

Red

External Trip

An external device has instructed the controller to trip the switchgear.

b-6

Red

Operator Trip

A local or remote operator has tripped the recloser.

Column C

c-1

Orange

A Phase Live

The source or load side bushing of the relevant phases are live.

c-2

Orange

B Phase Live

c-3

Orange

C Phase Live

 

c-4

Red

Load Current ON

Red when a load current greater than 2 A is flowing through the switchgear.

c-5

Green

System OK

The controller is functioning normally. Maintenance may be required when the lamp is flashing red. Consult the Event Log.

c-6

Green

AC Power

Flashing Red lamp when Auxiliary is OFF.

c-7

Green

Battery

Flashing Red lamp when Battery is OFF, not detected or test failed.

c-8

Red

Alarm

Flashing Red lamp when Trip or Close circuits are isolated, contact life is low or the switchgear is locked.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.