PKR39809-02

NPS Directional Protection

NOTE: NPS protection is not available by default. Sequence Components must be made available before it can be used The direction of NPS overcurrent faults can be determined by their Fault Angle.

The Fault Angle is the relationship between the NPS current INPS and the NPS voltage VNPS. that is VNPS → INPS

for example, VNPS = 60°, INPS = 180° Therefore NPS Fault Angle = 120°

NPS Voltage (VNPS) is used as the polarising voltage for NPS faults.

Operational values for directional NPS are shown below:

Polarising Method

Fault Angle

Characteristic Fault Angle (default)

Low Threshold (default)

Range

VNPS

VNPS→ INPS

120°

VNPS= 500 V

Adjustable VNPS300 to 2000 V

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.