PKR39809-02

USB-1, USB-2, and USB-3

At the time of writing, these ports can only be used with USB to RS232 converters. In which case their configuration and operation is similar to the IOEX/WSOS port.

The main differences being:

  • No application is running on these ports by default

  • Their default Mode is Remote

  • Their default Baud Rate is 115200

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.