PKR39809-02

System Frequency

The System Frequency can set corresponding to the frequency of the system where the device is installed. The options are:

  • 50 Hz

  • 60 Hz

In WSOS the system frequency is selected on the Measurement page.

Display > Measurement

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.