PKR39809-02

Protection Settings

Protection settings are also password protected. They differ from other password protected settings in that if the setting being changed is in the active protection group, a two-step process is required to put the changed setting into service. Until they are put into service, changed settings are saved. This allows several changes can be saved and put into service together.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.