PKR39809-02

Example

The example shown below is an PMSet N Series switchgear with the 1 side connected to the source. In this case power flow in the 1 side and out the 2 side would be positive and require the Power Direction to be set for
Source 1 > Load 2 as shown.

Figure 112
Power Direction setting according to orientation of the switchgear

The Power Flow Direction can also be configured on the operator interface.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.