PKR39809-02

Derived Values

The controller uses the measured values to derive many system measurements including:

  • Earth current

    • The vector sum of the three phase currents on three phase switchgear.

  • Frequency

    • The frequency of the voltage on the source and load sides of the switchgear.

  • Phase to phase voltages

    • Calculated from the phase to earth voltages.

  • Total and per phase power (kW, kVA, kVAR)

    • Calculated from the phase currents and phase to earth voltages according to the designated power direction.

  • Total and per phase PF

    • Calculated from the phase relationship between current and voltage phasors.

  • Harmonics

    • Second to sixteenth harmonic plus total harmonic distortion for voltage and current.

  • Sequence components

    • Positive Phase Sequence (PPS), NPS and Zero Phase Sequence (ZPS) voltages as well as PPS and NPS currents.

The PowerLogic ADVC Controller can also measure the internal values listed below:

  • CAPE temperature

  • Switchgear temperature on PMSet U Series and PMSet UR Series Circuit Breakers

  • Auxiliary voltage

  • Gas pressure on RL Series switchgear

  • Battery voltage

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.