PKR39809-02

Frequency

Engineer Menu> Measurements Menu> Frequency.

Displays the frequency of the voltage on the designated frequency bushing as well as separate frequency measurements for the source and load sides if available.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.