PKR39809-02

Current

Displays phase and earth current amplitudes and angles with respect to their corresponding voltages. PPS and NPS currents magnitude and angles are also displayed if sequence components are available.

  • A phase current and the angle with respect to A phase-earth voltage

  • B phase current and the angle with respect to B phase-earth voltage

  • C phase current and the angle with respect to C phase-earth voltage

  • Earth current and the angle with respect to the ZPS voltage.

  • PPS current and the angle with respect to the PPS voltage (if sequence components are available).

  • NPS current and the angle with respect to the NPS voltage (if sequence components are available).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.