PKR39809-02

RS232 Modem

This RS232 Modem port supports RTS, CTS, DTR, and DCD handshaking lines as well as Collision Avoidance. It is suitable for connection to conventional modems with flow control features that require that support.

The mode is Remote by default but can be configured as Local if required. The factory assigned default baud rate is 115200.

This port uses a standard 9 pin D male socket with the following pin connections.

Table 13 RS-232 Modem Port Pin Connections

Pin No.

Direction

Use

1

To ADVC

DCD

2

To ADVC

RxD

3

From ADVC

TxD

4

From ADVC

DTR

5

-

0 V (ground/earth)

6

-

Not connected

7

From ADVC

RTS

8

To ADVC

CTS

9

-

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.