PKR39809-02

Plant Details

The purpose of the plant details display is to provide information about the device that might be relevant to an operator or commissioning technician.

Plant details need to be made available through WSOS Feature Selection at:

Display > Configuration > Feature Selection > General.

Plant details can also be made available for ACR or AS on the O.I.

When available, Plant details can be entered on the status page in WSOS and are displayed on the Plant Details in the system status menu on the setVUE O.I.

The details entered can be American Standard Code for Information Interchange (ASCII) text or numbers limited to 90 characters.

NOTE: Plant details are not displayed on the flexVUE O.I.

The WSOS status page is shown below with plant details in the bottom left hand corner.

Figure 43
WSOS Status page

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.