PKR39809-02

Ultra

 
 

Stainless steel/Mild steel

3–Point locking

2 customer trays

Dimensions

Cubicle height 960 mm

Cubicle width 463 mm

Cubicle depth 352 mm

Figure 2
Ultra cubicle with flexVUE O.I.

Figure 3 shows an PowerLogic ADVC Controller with a flexVUE O.I. housed in an Ultra cubicle. The door is held open by the door stay mechanism. The standard equipment tray can be seen against the left hand wall and the additional equipment tray can be seen at the top of the cubicle. The 3-point locking mechanism on the door is also visible.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.