PKR39809-02

Appendix D ­ IEC255 Inverse Time Tables

The times shown for the inverse time curves in this appendix are calculated according to the formulas defined in the IEC 255 Standard.

  • Standard Inverse (SI) = 0.14 / (I^0.02-1)

  • Very Inverse (VI) = 13.5 / (I-1)

  • Extremely Inverse (EI) = 80 / (I^2-1)

Where I is the fault current expressed as a multiple of the setting current.

Each curve is defined in terms of a formula such as:

Time = T / (IN – Q) + B

Where:

T = time parameter specific to characteristic

I = ratio of fault current to setting current

N = parameter specific to characteristic

Q = parameter specific to characteristic

B = parameter specific to characteristic

Tables for the calculated times for each of the IEC255 curves are shown in the table below.

Table 104 IEC 255 Inverse Curves Timing Table

Setting Current Multiple

Standard Inverse Time (s)

Very Inverse Time (s)

Extremely Inverse Time (s)

1.10

73.37

135.00

380.95

1.50

17.19

27.00

64.00

2.00

10.03

13.50

26.67

2.50

7.57

9.00

15.24

3.00

6.30

6.75

10.00

3.50

5.52

5.40

7.11

4.00

4.98

4.50

5.33

4.50

4.58

3.86

4.16

5.00

4.28

3.38

3.33

5.50

4.04

3.00

2.74

6.00

3.84

2.70

2.29

6.50

3.67

2.45

1.94

7.00

3.53

2.25

1.67

7.50

3.40

2.08

1.45

8.00

3.30

1.93

1.27

8.50

3.20

1.80

1.12

9.00

3.12

1.69

1.00

9.50

3.04

1.59

0.90

10.00

2.97

1.50

0.81

10.50

2.91

1.42

0.73

11.00

2.85

1.35

0.67

11.50

2.80

1.29

0.61

12.00

2.75

1.23

0.56

12.50

2.70

1.17

0.52

13.00

2.66

1.13

0.48

13.50

2.62

1.08

0.44

14.00

2.58

1.04

0.41

14.50

2.55

1.00

0.38

15.00

2.52

0.96

0.36

15.50

2.48

0.93

0.33

16.00

2.46

0.90

0.31

16.50

2.43

0.87

0.29

17.00

2.40

0.84

0.28

17.50

2.38

0.82

0.26

18.00

2.35

0.79

0.25

18.50

2.33

0.77

0.23

19.00

2.31

0.75

0.22

19.50

2.29

0.73

0.21

20.00

2.27

0.71

0.20

20.50

2.25

0.69

0.19

21.00

2.23

0.68

0.18

21.50

2.21

0.66

0.17

22.00

2.20

0.64

0.17

22.50

2.18

0.63

0.16

23.00

2.16

0.61

0.15

23.50

2.15

0.60

0.15

24.00

2.13

0.59

0.14

24.50

2.12

0.57

0.13

25.00

2.11

0.56

0.13

25.50

2.09

0.55

0.12

26.00

2.08

0.54

0.12

26.50

2.07

0.53

0.11

27.00

2.05

0.52

0.11

27.50

2.04

0.51

0.11

28.00

2.03

0.50

0.10

28.50

2.02

0.49

0.10

29.00

2.01

0.48

0.10

29.50

2.00

0.47

0.09

30.00

1.99

0.47

0.09

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.