PKR39809-02

LOP Protection Settings

LOP protection is always available but can be selected Off if not required.

LOP protection can be in one of three operating modes:

  • OFF

  • Trip

  • Alarm

Table 58 LOP Protection Settings

LOP Setting

Description

Off

LOP protection is non-operational

Trip

LOP protection operation will trip the switchgear

Alarm

LOP protection operation will not cause the switchgear to trip. Instead an alarm will be recorded in the Event Log and can be reported via a SCADA protocol or via an IOEX output, flexVUE status lamp etc.

Once LOP protection has been set to either Trip or Alarm it will operate according to two settings:

  • LOP Voltage

    • The phase to earth voltage on one or two phases must fall below to start the LOP timer.

  • LOP Timeout

    • The time a LOP condition exists before either a protection trip occurs or an alarm is generated.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.