PKR39809-02

EF Directional Protection

When EF Directional Protection is enabled, it can use one of three methods to determine the direction of an EF.

  • VZPS

  • Wattmetric

  • Ir Cos (Ø)

VZPS is the default option. The Decision setting determines the method used. Operating Quantities, Fault Angles and default Characteristic Angles for each method are shown in the table below.

Table 51 Directional Protection EF Polarization Methods

Polarising Method (Decision)

Operating Quantity

Fault Angle

Angle logged on Trip

Default Characteristic Angle

VZPS

Earth Current Ir (IZPSx3)

VZPS →IZPS

VZPS → IZPS

135° Configurable

Wattmetric

Residual Power

(VZPSx3) x (IZPSx3) x Cos (FA)

VZPS → IZPS

VZPS → IZPS

180° Fixed

Ir Cos (Ø)

Active Earth Current

(IZPSx3) x Cos (FA)

VZPS → IZPS

VZPS → IZPS

180° Fixed

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.