PKR39809-02

Lamp Data

Printed labels are provided to identify each status lamp but additional data for each lamp can be displayed on the LCD by pressing the LAMP DATA key. In LAMP DATA mode, the arrow keys can be used to navigate to the status lamp of interest and display the additional information.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.