PKR39809-02

Firmware identification system

The firmware running in the PowerLogic ADVC Controller Range is identified by its version which has the form

AXX-XX.XX.

For example, A50-01.02 would be version 50.

This precisely identifies the firmware loaded into the program memory on the controller.

In order to obtain effective technical support from the manufacturer or your distributor it is vital to record the firmware version and to quote this when making any enquiries.

Without this information it is impossible for our customer service department to identify the firmware and provide the correct support.

The firmware version can be found on the setVUE O.I. on the Switchgear Wear/General Details and on the flexVUE O.I. in the Table 125 flexVUE Switchgear Info menu.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.