PKR39809-02

Using the Quick Keys

If a setting is to be changed via the Quick Keys, no other keys on the O.I. need to be used.

Example: If the controller is in Local mode and it is required to change to remote control mode, press the Local/Remote key. That will cause that setting to appear on the screen in change mode (flashing). Every time the Local/Remote key is pressed, the setting will toggle between local and RM. When remote is displayed, press the Enter key.

If the Prot Group key is being used to change the active protection group and more than two protection groups are configured, pressing that key will cause the display to cycle through the available groups.

NOTE: The Enter key on the Quick Keys pad has the same function as the Menu key.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.