PKR39809-02

Appendix K.5 ­ setVUE ACR and AS Communications Menu Screens

This appendix shows all of the Communications display group pages and lists display options and setting ranges.

The basic Communications display group consists of 28 (ADVC) default pages.

Up to 17 additional pages 13 (ADVC) can be added to the communications menu depending on the features that have been enabled.

Table 144 setVUE Communications Menu Pages for ACR and AS

Communications Menu

Sub-Menu

   

Defaults

Additional

Level 1

Level 2

Configure Ports (ADVC)

 

IOEX/WSOS

IOEX/WSOS 1

   

IOEX/WSOS2

 

Modem

Modem 1

   

Modem 2

   

Modem 3

   

Modem 4

 

Port-10BaseT

10BaseT

   

10BaseT Statistics

 

Port-10BaseT2

10BaseT 2

   

10BaseT 2 Statistics

 

USB-Port-1

USB-1

 

USB-Port-2

USB-2

 

USB-Port-3

USB-3

WSOS

 

WSOS Communications

 

WSOS Communications Statistics

DNP3

 

DNP Communications

 

DNP Communications Statistics

 

DNP Transmission Services 1, 2

 

DNP Unsolicited 1, 2, 3

 

DNP Diagnostics 1, 2

 

DNP Database Configuration

Trace Port

 

Communications Trace

   

Communications Trace Statistics

 

I101/4(1)

IEC 870-101 Communications

   

IEC 870-101 Communications Statistics

   

IEC 870-101 Transmission Services 1

   

IEC 870-101 Transmission Services 2

   

IEC 870-101 Transmission Services 3

   

IEC 870-101 Configuration 1

   

IEC 870-101 Configuration 2

 

Modbus(2)

Modbus Communications

   

Modbus Communications Statistics

 

MITS(3) (ADVC2 only)

MITS Communications

   

MITS Communications Statistics

   

MITS Transmission Data

   

MITS Time Configuration

 

NTP Communications/Servers

NTP Communications

   

NTP Servers

 

Radio Data Interface(4)

RDI Driver Communications

   

RDI Communications Statistics

(1) Only displayed when IEC 60870-5-101/104 is available.

(2) Only displayed when Modbus is available.

(3) Only displayed when MITS is available.

(4) Only displayed when Radio Data Interface Driver is available.

The communications menu is different from the other menus on the setVUE O.I. which means that it cannot be navigated from the first page using the Left or Right Arrow keys.

Each field on the first page is actually a sub-menu which must be selected and then entered before normal navigation can take place.

The first page displayed in the Communications menu is the Communications Setup page shown below.

Communications Setup 1

To enter one of the sub-menus displayed, navigate to it using the Select key and press Menu. Once the selected sub-menu has been entered it can be navigated in the normal manner.

The top line of each page is the page title. To the right of the title is the letter C which indicates that the page being displayed is part of the Communications display group.

The next three lines are the data or information on display. Most displays have six data fields. The standard layout is shown below.

If the standard menu is running, the protection menu can be accessed by pressing the Panel On key and then pressing the Menu key four times.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.