PKR39809-02

Live Load Blocking Operation

If Live Load Blocking is On, all close requests, manual or automatic, will be disregarded if any load side bushing is live.

An O.I. close request that is denied by Live Load Blocking will generate the following events:

  • Panel Close Request

  • Live Load Blocking

  • Operation Denied

Live Load Blocking Settings/Specifications

Live Load Threshold Voltage

2...15 kV

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.