PKR39809-02

Overview

The configurable IOEX tool allows WSOS users to generate custom I/O mappings for an IOEX.

Logic can be applied to each point with up to five sets of logic or actions for each input and one trigger action for each output.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.