PKR39809-02

Technical Manual

When the Protocol Configuration Tool opens, a new menu entitled protocol configuration tool will appear in the WSOS main menu bar.

From this menu, the technical manual for the protocol configuration tool can be opened from:

Protocol Configuration Tool Help> Manual.

Protocol technical manuals are also available from the help menu.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.