PKR39809-02

LOP versus Supply Timeout Example

Consider a situation where the following settings are applied:

  • LOP Protection – Trip

  • LOP Voltage – 2000 V

  • LOP Timeout – 10.0 s

  • Live Line Threshold – 2000 V

  • Supply Timeout – 4.0 s

And on a feeder energized at 6300 V per phase to earth, A phase goes dead at 00:00:00.00

The following events would be logged:

Time

Event

Cause

00:00:04.00

A1 Dead

A phase bushings recorded as dead when Supply Timeout expires after 4s.

00:00:04.00

A2 Dead

00:00:10.00

A Phase LOST

LOP protection operates 6 s later when the LOP Timeout expires.

00:00:10.00

Protection Trip Request

LOP issues a trip request to the switchgear.

The same sequence of events are shown in the timing diagram below.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.