PKR39809-02

Event Sources

The source of an event can vary. For example, a Work Tag Applied/OFF setting change event could have been triggered from IOEX, the O.I, local WSOS, remote WSOS over Ethernet, or a SCADA protocol.

The source of individual events can be seen in an abbreviated format by pressing the EVENT LOG key while the Event Log is displayed. This will add a fourth screen to each line of the Event Log which can be displayed by pressing the Right Arrow key. The additional screen provides space for setting change details.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.