PKR39809-02

DNP3

There is a five step procedure required in order to enable the PowerLogic ADVC Controller to communicate with a SCADA master station using the DNP3 protocol:

  1. Check that DNP3 is available.

  2. Select a communications port for DNP3.

  3. Configure the communications settings for the selected port.

  4. Assign the selected port to DNP3.

  5. Configure the DNP3 settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.