PKR39809-02

Per Element Protection

This feature provides the operator with the option of selecting to generate an alarm or trip an ACR on a per element basis. All protection elements encapsulated under the Phase Over current, EF, SEF and NPS protection can each be individually configured to:

  • Alarm Only

  • Trip

  • Off

When any element is configured to Alarm only, a protection operation will not trip the switchgear, but only register an alarm.

When Extended Standard Protection is also enabled, it provides the operator the option to configure different Trip and Alarm settings on a per group basis.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.