PKR39809-02

IOEX Available

The PowerLogic ADVC Controller can support two IOEX devices but the first IOEX must be made available either through WSOS feature selection:

Display> Configuration> Feature Selection> General
or through the operator interface.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.