PKR39809-02

flexVUE Customisation

Figure 47
flexVUE O.I. layout

The flexVUE O.I. has the following configurable lamps and keys:

  • 20 Status Lamps (a1 – c8)

  • 12 QAK with imbedded LED’s (d1 – f4)

Each of the functions below are fully configurable as well:

  • Trip and Trip Disabled

  • Close and Close Disabled

  • Quick Action Key Unlock

The OCP Configuration Tool which can be launched from WSOS is a software tool provided for this purpose. For details of how to launch the OCP Configuration Tool, refer to Launching the OCP Configuration Tool in PC Software (WSOS).

Figure 48
flexVUE O.I.

The OCP Configuration Tool can be used to configure/customize the following:

  • The function of the Status Lamps and QAK.

  • The Description of Status Lamps and QAK.

  • The Lamp color for TRUE/FALSE state.

  • Flashing of lamps.

  • Locking of QAK.

  • Set QAK Active when the O.I. is OFF.

  • Display status of Status lamps and Quick Action Key lamps when the O.I. is OFF.

  • Set TRIP and CLOSE buttons active when the O.I. is OFF

    .
  • Delay operation of TRIP and CLOSE buttons.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.