PKR39809-02

Updating Controller Firmware

The PowerLogic ADVC Controller supports firmware versions 50+. PowerLogic ADVC Controller files have an .advc extension.

Updating the firmware in an PowerLogic ADVC Controller can be carried out through WSOS by using the procedure below or via USB Memory Stick.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.