PKR39809-02

Appendix K.3 ­ setVUE ACR and AS Measurement Menu Screens

This appendix shows all of the Measurement display group pages and lists display options and setting ranges.

The real time or instantaneous measurements appear at the start of the menu, followed by supply outage information, sag and swell monitoring with historical records at the end.

The basic Measurement display group consists of nine default pages.

Up to six additional pages can be added depending on the features that have been enabled.

The table below shows a complete list of available pages and their position in the measurement menu.

Table 142 setVUE Measurement Pages for ACR and AS

Measurement Menu

Default pages

Additional pages

System Measurements

 

Current

 

Voltage

 
 

Sequence Voltage(1)

Frequency

 

Power

 
 

Synchronization(2)

 

Supply Outages(3)

 

Sag/Swell Monitoring(4)

 

Sag Monitoring(4)

 

Swell Monitoring(4)

Daily Maximum Demand

 

Weekly Maximum Demand

 

Monthly Maximum Demand

 

Maximum Demand Indicator

 

(1) Sequence components available.

(2) Sync check available.

(3) Supply outages available.

(4) Sag/Swell available.

The top line of each page is the page title. To the right of the title is the letter M which indicates that the page being displayed is part of the Measurement display group.

The next three lines are the data on display. Most displays have six data fields. The standard layout is shown below.

Where details of individual pages are shown below a small column has been added to the right of each field to indicate the type of data displayed. The letters in this column have significance as follows:

O Operator Controlled

D Display Only (that is cannot be changed)

P Password Protected (that is cannot be changed unless the password is entered)

R Operator Controller Reset (that resets a field or group of fields)

If the standard menu is running, the measurement menu can be accessed by pressing the Panel On key and then pressing the Menu key two times.

The first page to be displayed in the Measurement menu is the System Measurements page shown below.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.