PKR39809-02

Average Phase Logic Events

When the Phase Logic is set to Average, only one event is logged for Voltage High and Low events as well as Minimum and Maximum voltage events.

Examples are shown below:

  • ABC Voltage High

  • ABC Voltage Low

  • ABC Min 0.84 pu

  • ABC Max 1.16 pu

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.